Hi Nivas B,
If your target is the Cortex M4 processor, then you can refer to the K64 opensda source code:
OpenSDA Serial and Debug Adapter | NXP
You can assign two pin in the RT, one as SWD_CLK, one as SWD_DIO, then simulate the SWD interface sequence.
This application note maybe also useful to you:
https://www.nxp.com/docs/en/application-note/AN4835.pdf?fsrch=1&sr=1&pageNum=1
About the specific programmer with RT chip, and the program target is the M4 core, we don't have that application code for your reference, you need to design it by yourself, actually, it is the specific application design.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------