SRAM CS definition in i.MXRT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SRAM CS definition in i.MXRT1170

跳至解决方案
2,032 次查看
Eugene3
Contributor II

There are some wordings about SRAM chip select in the i.MXRT1170 reference manual.

"SRAM CE# X" is used on IOCR section.

"SRAM CS X" is used on BRn section.

"SRAM device X" is used on SRAMCRn section.

Are "SRAM CE# 0", "SRAM CS 0" and "SRAM device 0" same meaning?

  

 

0 项奖励
回复
1 解答
1,979 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,991 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SRAM CE# is used as there are some pins that can optionally be configurable as Chip Enable.
In BRn CS is referred to as SRAM devices that can be connected to SEMC, as you know you can connect up to 4 devices with 4 different CS.
SRAM CSn can be used to refer to a specific device e.g. CS0 is used in SRAM device 0; while CE# refers specifically to the ChipEnable signal.

Best regards,
Omar

0 项奖励
回复
1,987 次查看
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you for your kindly answer.

CSn is used in SRAM device n, and its ChipEnable signal is CE# n.

n = 0 to 3.

Is my understanding correct?

0 项奖励
回复
1,980 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

0 项奖励
回复
1,972 次查看
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you. I completely understand.

 

0 项奖励
回复