SRAM CS definition in i.MXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRAM CS definition in i.MXRT1170

Jump to solution
2,106 Views
Eugene3
Contributor II

There are some wordings about SRAM chip select in the i.MXRT1170 reference manual.

"SRAM CE# X" is used on IOCR section.

"SRAM CS X" is used on BRn section.

"SRAM device X" is used on SRAMCRn section.

Are "SRAM CE# 0", "SRAM CS 0" and "SRAM device 0" same meaning?

  

 

0 Kudos
Reply
1 Solution
2,053 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
4 Replies
2,065 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SRAM CE# is used as there are some pins that can optionally be configurable as Chip Enable.
In BRn CS is referred to as SRAM devices that can be connected to SEMC, as you know you can connect up to 4 devices with 4 different CS.
SRAM CSn can be used to refer to a specific device e.g. CS0 is used in SRAM device 0; while CE# refers specifically to the ChipEnable signal.

Best regards,
Omar

0 Kudos
Reply
2,061 Views
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you for your kindly answer.

CSn is used in SRAM device n, and its ChipEnable signal is CE# n.

n = 0 to 3.

Is my understanding correct?

0 Kudos
Reply
2,054 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

0 Kudos
Reply
2,046 Views
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you. I completely understand.

 

0 Kudos
Reply