SRAM CS definition in i.MXRT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRAM CS definition in i.MXRT1170

ソリューションへジャンプ
2,081件の閲覧回数
Eugene3
Contributor II

There are some wordings about SRAM chip select in the i.MXRT1170 reference manual.

"SRAM CE# X" is used on IOCR section.

"SRAM CS X" is used on BRn section.

"SRAM device X" is used on SRAMCRn section.

Are "SRAM CE# 0", "SRAM CS 0" and "SRAM device 0" same meaning?

  

 

0 件の賞賛
返信
1 解決策
2,028件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,040件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

SRAM CE# is used as there are some pins that can optionally be configurable as Chip Enable.
In BRn CS is referred to as SRAM devices that can be connected to SEMC, as you know you can connect up to 4 devices with 4 different CS.
SRAM CSn can be used to refer to a specific device e.g. CS0 is used in SRAM device 0; while CE# refers specifically to the ChipEnable signal.

Best regards,
Omar

0 件の賞賛
返信
2,036件の閲覧回数
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you for your kindly answer.

CSn is used in SRAM device n, and its ChipEnable signal is CE# n.

n = 0 to 3.

Is my understanding correct?

0 件の賞賛
返信
2,029件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Your understanding is correct.
It is important to clarify that CE and CS make reference to the same signal.

Best regards,
Omar

0 件の賞賛
返信
2,021件の閲覧回数
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you. I completely understand.

 

0 件の賞賛
返信