I have the MIMXRT1060-EVKB board. I note on the Zephyr page for MIMXRT1060-EVK (not B) in mentions to use SPI it is necessary to solder zero ohm resistors at R278, R279, R280 and R281.
Questions about SPI resistors:
Am I also required to solder the resistors on MIMXRT1060-EVKB (B revision) board?
Is there a diagram that shows the location of these resistors, there are literally hundreds of them!
Questions about Zephyr Samples:
I am planning on developing with Zephyr 3.5.0. Should I expect samples such as samples/basic/blinky to work and actually blink the LED. My initial test on 3.6.0, the LED did not blink. Does it require some additional devicetree configuration to enable the LED?
Questions about Zephyr Board configuration:
I need to run the SPI interface clock at 50 MHz. What is the default SPI clock rate and what are the configurable options? Should I modify the configuration in device tree or is there a way to do it at runtime?
thank you for your support!
解決済! 解決策の投稿を見る。
Thanks a lot for your patience.
Yes, to enable SPI on J17 you need to solder those resistors.
By the way to find resistors, I usually see the layout printed on a PDF. Download the RT1060-EVKB design files and navigate to this path MIMXRT1060-EVKB-DESIGN-FILES.zip\MIMXRT1060-EVKB-DESIGNFILE-RevB1\Layout
I hope this helps you!
Diego
Can these SPI pins be configured to connected to the full speed FlexSPI or only to the LPSPI? My application has a large amount of data to transfer and needs the maximum SPI speed available. Are the MIMXRT1062 pins fully configurable to any peripheral or are they more limited?
RT1xxx pins have limited pin mux options. Pin mux options for peripherals can be seen in the Table 10-1. Muxing Options of the RT1062 reference manual. Sometimes, I prefer to use our MCUXpresso Config Tools Pins tool to understand pin mux options with ease.
Best regards,
Diego
Thanks a lot for your patience.
Yes, to enable SPI on J17 you need to solder those resistors.
By the way to find resistors, I usually see the layout printed on a PDF. Download the RT1060-EVKB design files and navigate to this path MIMXRT1060-EVKB-DESIGN-FILES.zip\MIMXRT1060-EVKB-DESIGNFILE-RevB1\Layout
I hope this helps you!
Diego