I have the MIMXRT1060-EVKB board. I note on the Zephyr page for MIMXRT1060-EVK (not B) in mentions to use SPI it is necessary to solder zero ohm resistors at R278, R279, R280 and R281.
Questions about SPI resistors:
Am I also required to solder the resistors on MIMXRT1060-EVKB (B revision) board?
Is there a diagram that shows the location of these resistors, there are literally hundreds of them!
Questions about Zephyr Samples:
I am planning on developing with Zephyr 3.5.0. Should I expect samples such as samples/basic/blinky to work and actually blink the LED. My initial test on 3.6.0, the LED did not blink. Does it require some additional devicetree configuration to enable the LED?
Questions about Zephyr Board configuration:
I need to run the SPI interface clock at 50 MHz. What is the default SPI clock rate and what are the configurable options? Should I modify the configuration in device tree or is there a way to do it at runtime?
thank you for your support!