SPI communication at 32 bits per frame

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI communication at 32 bits per frame

1,087 Views
oindrila14
Contributor I

I am working with EVK mimxrt 1020 board. I am trying to achieve SPI communication with eDMA at at rate of 32 bits per frame. But it looks like the eDMA library for master transmit in the SDK examples is made for communication at 8bits per frame. Has anybody tried this and knows how this can be made possible?

0 Kudos
Reply
1 Reply

1,083 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi oindrila14,

   Yes, you are right, the RT1020 LPSPI DMA project is configured as 8bits per frame, but it doesn't mean you can't use the 32bits per frame, as you know, the LPSPI register also can support 32 bit per frame, you can configure the LPSPI modules as 32 bit perframe.

  In the default LPSPI_MasterGetDefaultConfig, you can find the LPSPI is configuring the bitperframe =8, you can change it. and you also can check other DMA related area, change the 8 bits to 32 bits.

   You can try it.

  If you still have issues, just kindly let me know.

Best Regards,

kerry

0 Kudos
Reply