SLN-VIZNAS-IOT Camera Lenses

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SLN-VIZNAS-IOT Camera Lenses

1,553 次查看
MRota
Contributor I

I need to replace the standard lenses with different ones.

Do you know what are the screw-thread specifications of the installed mount?

It seems to be either M5 or M6, but the pitch is also needed.

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,539 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello MRota,

Are you referring to the lenses of the Dual Camera module itself? This whole module is marked as manufactured by Ningbo Jinshengxin with part number MT03-0CCM-D3. It has two OnSemi MT9M114

Sensors and is shipped as is for the SLN-VIZNAS-IOT, so while you may be able to disassembly the module, we do not have sub assembly information.

The dual camera module itself is glued on top of the vision adapter board.

My apologies for the inconvenience.

Regards,
Gustavo

0 项奖励
回复

1,419 次查看
accatpaliz
Contributor II

Do you have any datasheet of MT03-0CCM-D3 ? I need dimensions (distance between lenses and lens diameter , ...)

0 项奖励
回复