SLN-VIZNAS-IOT Camera Lenses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SLN-VIZNAS-IOT Camera Lenses

1,880 Views
MRota
Contributor I

I need to replace the standard lenses with different ones.

Do you know what are the screw-thread specifications of the installed mount?

It seems to be either M5 or M6, but the pitch is also needed.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,866 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello MRota,

Are you referring to the lenses of the Dual Camera module itself? This whole module is marked as manufactured by Ningbo Jinshengxin with part number MT03-0CCM-D3. It has two OnSemi MT9M114

Sensors and is shipped as is for the SLN-VIZNAS-IOT, so while you may be able to disassembly the module, we do not have sub assembly information.

The dual camera module itself is glued on top of the vision adapter board.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply

1,746 Views
accatpaliz
Contributor II

Do you have any datasheet of MT03-0CCM-D3 ? I need dimensions (distance between lenses and lens diameter , ...)

0 Kudos
Reply