Hello,
I wanted to know if anyone had a chance to try out a different camera with higher resolution on the SLN-VIZN-IOT board. Something in the range of 2MP.
Hello,
Currently the MT9M114 and GC0308 are the only ones we have officially tested. It's possible that a similar image sensor like the OV7725 would work, but we can't guarantee that at the moment as it's not something we've tested. In general for camera requirements, the solution needs a sensor which supports a DVP interface, RGB or YUV data output, and should support VGA resolution.
Hope it help you. Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
Thank you for your reply,
Are you planning to update the camera module to a higher resolution ? Are you working on a new Camera module ?
Looking forward for your reply
Thanks
Netanel
Hello,
Thanks for your feedback. Unfortunately, There is not the more information for it so far. Sorry for it.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------