SEMC Demo Project i.mxRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEMC Demo Project i.mxRT1050

1,862 Views
christiangradl
Contributor III

Hi, i 've just downloaded the semc demo project for i.mxrt1050. i think there is a very fatal mistake

void SEMC_GetDefaultConfig(semc_config_t *config)
{
    assert(config);

    semc_axi_queueweight_t queueWeight; /*!< AXI queue weight. */
    semc_queuea_weight_t queueaWeight;
    semc_queueb_weight_t queuebWeight;

    /* Get default settings. */
    config->dqsMode = kSEMC_Loopbackinternal;
    config->cmdTimeoutCycles = 0;
    config->busTimeoutCycles = 0x1F;

    /* Set a typical weight settings. */
    memset((void *)&queueWeight, 0, sizeof(semc_axi_queueweight_t));

    queueaWeight.qos = SEMC_BMCR0_TYPICAL_WQOS;
    queueaWeight.aging = SEMC_BMCR0_TYPICAL_WAGE;
    queueaWeight.slaveHitSwith = SEMC_BMCR0_TYPICAL_WSH;
    queueaWeight.slaveHitNoswitch = SEMC_BMCR0_TYPICAL_WRWS;
    queuebWeight.qos = SEMC_BMCR1_TYPICAL_WQOS;
    queuebWeight.aging = SEMC_BMCR1_TYPICAL_WAGE;
    queuebWeight.slaveHitSwith = SEMC_BMCR1_TYPICAL_WRWS;
    queuebWeight.weightPagehit = SEMC_BMCR1_TYPICAL_WPH;
    queuebWeight.bankRotation = SEMC_BMCR1_TYPICAL_WBR;

    config->queueWeight.queueaWeight = &queueaWeight;
    config->queueWeight.queuebWeight = &queuebWeight;
}

Both vars "queueaWeight" and "queuebWeight" are on the stack.

The function void SEMC_Init reads the pointers, etc., etc. etc.

How can this work? The content of the Stackmem is not saved....

Tags (1)
0 Kudos
Reply
4 Replies

1,564 Views
christiangradl
Contributor III

Hi, both variables are lying on the stack and with these pointer assignments they are used later in the code

    config->queueWeight.queueaWeight = &queueaWeight;
    config->queueWeight.queuebWeight = &queuebWeight;

it is not really safe to use the content of the stackmemory later anywhere in the code.

0 Kudos
Reply

1,564 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Christian,

In order to report any issue and the examples I need to demonstrate that it fails. If you can see a specific scenario which I can reproduce and show that it fails please let me know.

Carlos

0 Kudos
Reply

1,564 Views
christiangradl
Contributor III

Hi,

ok thats simple.

have a look to SEMC driver.

void SEMC_GetDefaultConfig(semc_config_t *config)
{
    assert(config);

    SEMC_AXI_QUEUEWEIGHT_TYPE queueWeight; // AXI queue weight.
    SEMC_QUEUEA_WEIGHT_TYPE queueaWeight;  // !!! Q0 !!!
    SEMC_QUEUEB_WEIGHT_TYPE queuebWeight;
    // Get default settings
    config->dqsMode = kSEMC_Loopbackinternal;
    config->cmdTimeoutCycles = 0;
    config->busTimeoutCycles = 0x1F;
    memset((void *)&queueWeight, 0, sizeof(SEMC_AXI_QUEUEWEIGHT_TYPE));        // !!! Q1 !!!
    queueaWeight.qos = SEMC_BMCR0_TYPICAL_WQOS;
    queueaWeight.aging = SEMC_BMCR0_TYPICAL_WAGE;
    queueaWeight.slaveHitSwith = SEMC_BMCR0_TYPICAL_WSH;
    queueaWeight.slaveHitNoswitch = SEMC_BMCR0_TYPICAL_WRWS;
    queuebWeight.qos = SEMC_BMCR1_TYPICAL_WQOS;
    queuebWeight.aging = SEMC_BMCR1_TYPICAL_WAGE;
    queuebWeight.slaveHitSwith = SEMC_BMCR1_TYPICAL_WRWS;
    queuebWeight.weightPagehit = SEMC_BMCR1_TYPICAL_WPH;
    queuebWeight.bankRotation = SEMC_BMCR1_TYPICAL_WBR;
    config->queueWeight.queueaWeight = &queueaWeight;                  // !!! Q2 !!!!
    config->queueWeight.queuebWeight = &queuebWeight;

}

void SEMC_Init(SEMC_Type *base, SEMC_CONFIG_TYPE *configure)
{

    .......
    // Configure Queue 0/1 for AXI bus

    // !!! Q3 !!!!
    if (configure->queueWeight.queueaWeight) base->BMCR0 = (unsigned long)(configure->queueWeight.queueaWeight);      if (configure->queueWeight.queuebWeight) base->BMCR1 = (unsigned long)(configure->queueWeight.queuebWeight);
}

ad !!! Q1 !!!

queueWeight is a local variable, where is this var used? I think it is dead code

ad !!! Q2 !!!

config->queueWeight.queueaWeight and config->queueWeight.queuebWeight  !!!!  are Pointers !!!!

ad !!! Q3 !!!

base->BMCR0 is set with the pointer address and not with the content ???? Why

ad !!! Q0 !!!

SEMC_QUEUEA_WEIGHT_TYPE queueaWeight is a local variable

at !!! Q2 !!! is then assign with the address if this local variable

at !!! Q3 !!! if the content should be used, then think about this.

    SEMC_GetDefaultConfig(&config);
    MyFunction();      // here the stack memory is used and content of queueaWeight and queuebWeight is being destoryed
    SEMC_Init(SEMC, &config);

christian

0 Kudos
Reply

1,564 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Christian,

which is the behavior you are facing?

Carlos

0 Kudos
Reply