SDRAM frequency test for 133MHZ clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDRAM frequency test for 133MHZ clock

跳至解决方案
1,388 次查看
anasnadukkandiyil
Contributor III

Hi team,

Please respond it is urgent.

We are working on imxrt1176 with SDRAM test code 

Could you please confirm that event if DCD and clock_config.c and ,h are having changes for new frequency 133mHZ/166MHZ?

 

and run a sample code of evkmimxrt1170_semc_cm7, effective frequency will be based on settings written in

 

 

status_t BOARD_InitSEMC(void)

{

semc_config_t config;

semc_sdram_config_t sdramconfig;

uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

 

/* Initializes the MAC configure structure to zero. */

memset(&config, 0, sizeof(semc_config_t));

memset(&sdramconfig, 0, sizeof(semc_sdram_config_t));

 

/* Initialize SEMC. */

SEMC_GetDefaultConfig(&config);

config.dqsMode = kSEMC_Loopbackdqspad; /* For more accurate timing. */

SEMC_Init(SEMC, &config);

 

/* Configure SDRAM. */

sdramconfig.csxPinMux = kSEMC_MUXCSX0;

sdramconfig.address = 0x80000000;

sdramconfig.memsize_kbytes = 2 * 32 * 1024; /* 64MB = 2*32*1024*1KBytes*/

sdramconfig.portSize = kSEMC_PortSize32Bit; /*two 16-bit SDRAMs make up 32-bit portsize*/

sdramconfig.burstLen = kSEMC_Sdram_BurstLen8;

sdramconfig.columnAddrBitNum = kSEMC_SdramColunm_9bit;

sdramconfig.casLatency = kSEMC_LatencyThree;

sdramconfig.tPrecharge2Act_Ns = 15; /* tRP 15ns */

sdramconfig.tAct2ReadWrite_Ns = 15; /* tRCD 15ns */

sdramconfig.tRefreshRecovery_Ns = 70; /* Use the maximum of the (Trfc , Txsr). */

sdramconfig.tWriteRecovery_Ns = 2; /* tWR 2ns */

sdramconfig.tCkeOff_Ns =

42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/

sdramconfig.tAct2Prechage_Ns = 40; /* tRAS 40ns */

sdramconfig.tSelfRefRecovery_Ns = 70;

sdramconfig.tRefresh2Refresh_Ns = 60;

sdramconfig.tAct2Act_Ns = 2; /* tRC/tRDD 2ns */

sdramconfig.tPrescalePeriod_Ns = 160 * (1000000000 / clockFrq);

sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */

sdramconfig.refreshUrgThreshold = sdramconfig.refreshPeriod_nsPerRow;

sdramconfig.refreshBurstLen = 1;

sdramconfig.delayChain = 2;

 

return SEMC_ConfigureSDRAM(SEMC, kSEMC_SDRAM_CS0, &sdramconfig, clockFrq);

}

 

 

if so what will be the settings for 133MHZ and 166MHZ SDRAM frequency?

0 项奖励
回复
1 解答
1,377 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @anasnadukkandiyil ,

DCD can set clock but BOARD_InitSEMC() can't. DCD is configured in dcd.c. When compile, it will be put in image header. The bootROM can read DCD sector and configure SEMC and clock.

BOARD_InitSEMC() can overwrite SEMC settings but not clock. The SDRAM clock is set in clock_config.c. SDRAM operation speed is same to SEMC clock root.

This picture is copy from MCUXpresso config tool. You can use it to config SDRAM clock easily.

jingpan_0-1675134580723.png

 

Regards,

Jing

在原帖中查看解决方案

1 回复
1,378 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @anasnadukkandiyil ,

DCD can set clock but BOARD_InitSEMC() can't. DCD is configured in dcd.c. When compile, it will be put in image header. The bootROM can read DCD sector and configure SEMC and clock.

BOARD_InitSEMC() can overwrite SEMC settings but not clock. The SDRAM clock is set in clock_config.c. SDRAM operation speed is same to SEMC clock root.

This picture is copy from MCUXpresso config tool. You can use it to config SDRAM clock easily.

jingpan_0-1675134580723.png

 

Regards,

Jing