SDRAM ECC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,115件の閲覧回数
Ootsuka
Contributor II

Hello teams.

We designed an i.MX RT1171 custom board and connect it to the SDRAM on the SEMC bus.
Please tell us how to enable ECC.

We enabled XECC_SEMC[ECC_CTRL] bit2-0 and address settings, but it doesn't work.
Must be set to the eFUSE 0x840[3] bit?
Is there any other settings ?

Best regards.

タグ(3)
0 件の賞賛
返信
1 解決策
2,099件の閲覧回数
jay_heng
NXP Employee
NXP Employee

eFUSE 0x840[3] bit should be burnt to enable XECC module, or XECC is inactive by default.

See my blog for XECC enablement.

https://www.cnblogs.com/henjay724/p/15204125.html

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,096件の閲覧回数
Ootsuka
Contributor II

Thank you very much for answer.

0 件の賞賛
返信
2,100件の閲覧回数
jay_heng
NXP Employee
NXP Employee

eFUSE 0x840[3] bit should be burnt to enable XECC module, or XECC is inactive by default.

See my blog for XECC enablement.

https://www.cnblogs.com/henjay724/p/15204125.html

0 件の賞賛
返信