Reduce the noise on CSI pin by the RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reduce the noise on CSI pin by the RT1060

Jump to solution
1,590 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello, all

 

Customer(Panasonic) wants to reduce the noise on the pin  of 「IOMUXC_GPIO_AD_B1_05_CSI_MCLK」by decline the drive strength by following two methods?

1. By setting the appropriate Rdrv impedance value  

ZHOU_XIAO_0-1645409252094.png

2 To change the prescaler of CSI_MCLK. The current prescaler is 1/2, and customer wants to change the prescaler to decline the strength of drive.

How about the two method?

@lucas_cao 

 

Best regars

ZHOU

Labels (1)
0 Kudos
Reply
1 Solution
1,561 Views
lucas_cao
NXP Employee
NXP Employee

Reduce the Drive strength values in pad settings will help on this.

View solution in original post

0 Kudos
Reply
3 Replies
1,581 Views
lucas_cao
NXP Employee
NXP Employee

Hi Zhou,

Does the noise here means RE noise? Could you pleae check this with customer?

if yes, i think the first question can be used. But i don't think the second one can reduce RE result.

0 Kudos
Reply
1,568 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello, @lucas_cao 

Does the noise here means RE noise? Could you pleae check this with customer?

→Yes.   The customer means RE(radiated emission) . They concerns about the RE of  the CSI MCLK.  and want to reduce the RE noise.

Currently , they measure the pin of CSI MCLK.

Although the power supply is 3.3 V , the amplitude of the CSI MCLK is about   -1.8 V ~~ 5.1V.

Do you have any comments about the  big the amplititude of -1.8 V ~~ 5.1V?

 

Best regards

ZHOU

 

 

 

 

0 Kudos
Reply
1,562 Views
lucas_cao
NXP Employee
NXP Employee

Reduce the Drive strength values in pad settings will help on this.

0 Kudos
Reply