Re: imxrt1010 SAI_TransferSendEDMA / SAI_TransferReceiveEDMA can't be used for ping-pong buffers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: imxrt1010 SAI_TransferSendEDMA / SAI_TransferReceiveEDMA can't be used for ping-pong buffers

2,590件の閲覧回数
bowerymarc
Contributor V

Hi Jeremy,

You need to try to build one of those demos using the code generated by the configuration tool.  Walk through it as I have.  You will find that the code pulled in by the config tool preclude the uses you claim they can.  You are clearly unfamiliar with the config tool code.

If the configuration tool is not able to provide for these common scenarios, your team needs to revise the tool, not tell your customers that it's useless. 

The older Kinetis tools were much more useful.  As are the ST Micro CubeMX.  NXP needs to step up it's game.

Best,

Marc

0 件の賞賛
返信
2 返答(返信)

2,406件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'll give it a try, and you'd better describe what exactly demo you want to create and demonstrate the steps of configuring the config tool you did.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,340件の閲覧回数
bowerymarc
Contributor V

you can try the sai demo app, or one of the USB audio apps.  They all have the same underlying driver code. 

thx

M

0 件の賞賛
返信