RTC_XTALI level for i.MX RT117x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC_XTALI level for i.MX RT117x

Jump to solution
978 Views
Ootsuka
Contributor II

Hello teams.

I'm trying to desiged i.MX RT1171 custum board.

What is the maximum level of RTC_XTALI at logic level clock input?
Please tell me which is the correct answer.(I think it's VDD_SNVS_ANA level...)

 

In section 3.1 of the Datasheet, RTC_XTALI / RTC_XTALO is described up to the VDD_SNVS_DIG level.

Table 4. Special signal considerations
--------
"If you want to feed an external low-frequency clock into RTC_XTALI, the RTC_XTALO pin must
remain unconnected or driven by a complementary signal. The logic level of this forcing clock must
not exceed the VDD_SNVS_DIG level"

 

But, in section 4.2.6 of the Datasheet, RTC_XTALI is described up to the VDD_SNVS_ANA level.

Table 32. 32 kHz oscillator DC electrical specifications Note 3
--------
"The voltage of the applied clock must be within the range of VSS to VDD_SNVS_ANA."

 

VDD_SNVS_ANA=1.75V
VDD_SNVS_DIG=0.85V
And VDD_SNVS_DIG is not output by default.

Best regards.

0 Kudos
Reply
1 Solution
966 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What is the maximum level of RTC_XTALI at logic level clock input?
--In my opinion, I agree with your idea, it's VDD_SNVS_ANA level.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
967 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What is the maximum level of RTC_XTALI at logic level clock input?
--In my opinion, I agree with your idea, it's VDD_SNVS_ANA level.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
963 Views
Ootsuka
Contributor II

Hello,

I am glad to inform you that the question is now solved.
I designed as VDD_SNVS_ANA level.

Thank you very much for answer.

0 Kudos
Reply