RT685 i3c port with Zephyr - driver with i2c devices dies after minutes of use

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT685 i3c port with Zephyr - driver with i2c devices dies after minutes of use

ソリューションへジャンプ
5,706件の閲覧回数
galenc
Contributor II

I have a system based around the MIMXRT685-EVK running Zephyr.  I have the i3c port configured and interfacing with a few i2c devices.  They all work for some time, but depending of frequency of communication the bus/driver will just die after a few minutes.

I experienced this on the evk and on our custom board.  And similarly with all the peripherals on the bus or just a single one. 

here you can see the scope (yellow SDA, green SCL, violet device interrupt) it just stops trying any comms on the bus when it should be servicing the interrupt:logic outputlogic output

It happens for this device which is imu - lsm6dso (a zephyr built in driver), sampling at higher frequency from interrupts. Even communicating with another device at slower frequency it will stay up longer but eventually crash (maybe 5-10 minutes with a polling message every second).

Here is the warnings we saw from the i3c_mcux driver just before the bus goes dead.  the errors are failed attempts to read from device registers (the bus in the scope has no activity from subsequent attempts, shown in red as errors):
warning from i3c_mcux before bus crashwarning from i3c_mcux before bus crash

Has anyone seen any issues similar with the i3c bus and zephyr implementation specifically?

our whole bus is essentially i2c devices we don't need the features of i3c (we are using it because we are using all the other ports) if there is a way it might be more stable if we "force" it into i2c mode all the time? 

It don't know if there is a bug in the driver or some way to better configure it?  we are using it pretty much as it came.  see device tree sections:

 

 

 

 

&i3c0 {
	status = "okay";

	i2c-scl-hz = <400000>;
	i3c-scl-hz = <400000>;
	i3c-od-scl-hz = <400000>;

	clk-divider = <12>;
	clk-divider-slow = <1>;
	clk-divider-tc = <1>;

	pinctrl-0 = <&pinmux_i3c>;
	pinctrl-names = "default";

	lsm6dso0: lsm6dso@6a0000000000000050 {
		status = "okay";
		compatible = "st,lsm6dso";
		reg = <0x6a 0x00 0x50>;
		irq-gpios = <&gpio1 10 GPIO_ACTIVE_HIGH>;
	};
};
	pinmux_i3c: pinmux_i3c {
		group0 {
			pinmux = <I3C0_SCL_PIO2_29>,
					 <I3C0_SDA_PIO2_30>;
			input-enable;
			slew-rate = "slow";
			drive-strength = "high";
		};

		group1 {
			pinmux = <I3C0_PUR_PIO2_31>;
			slew-rate = "normal";
			drive-strength = "normal";
		};
	};

 

 

 

 


Any help is much appreciated.

Thanks, Galen 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
4,703件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Glad your I2C bitbang recover bus works. On the master side, several things you should check:

(1) PIN MUX needs to set back to I3C SCL and SDA lines.

(2) Make sure both MSTATUS and MERRWARN registers are reset to default state. 

(3) In our SDK code, we have a module called I3C_MasterTransferAbort() to abort the master transfer. Please take a close look on this. I don't know why you would stay in NORMACK state even after you have issued STOP request. After you emit stop, you should wait for CTRL DONE. Once CTRL DONE is seen, it should be back to IDLE state.

(4) If (2) and (3) don't work, I don't know what else you can do, maybe reset I3C by writing 1 to I3C0 bit in RSTCTL1_PRSTCTL2. You may want to check all the I3C registers, especially, MCONFIG and make sure they are the same before and after resetting I3C bit.  

 

元の投稿で解決策を見る

0 件の賞賛
返信
25 返答(返信)
1,220件の閲覧回数
galenc
Contributor II
Yes, I agree this is a good idea for debug. I will set this up. I will be traveling for the next two weeks (starting tomorrow) but will report my results when I return.

Thanks for your continued help on this issue.
0 件の賞賛
返信
1,242件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

I tried to isolate the problem if Zephyr OS causes the problem or not and have run a standalone test on the I2C device using I3C controller. Here is a what I have done: on RT685 EVK board, there is a codec WM8904 on the I3C bus, if you use any audio related SDK example, this codec will be initialized using I3C controller (over I2C), I made minor change to do register reading periodically, monitor the bus and have never seen timeout happened unless you force it into one of these conditions below. It doesn't look our I3C controller could time out easily unless the STALL period is > 100us.

TIMEOUT Time-out error. The module has stalled too long in a frame. This happens:
• When the TX FIFO or RX FIFO is not handled and the bus is stuck in the middle of a
message,
• When no STOP was issued and between messages,
• When IBI manual is used and no decision was made.
The maximum stall period is 10 kHz or 100 us.

It's hard to time how often bus recovery should be called, hopefully, investigate why timeout happens so often first.

I don't know about the IO error, it looks like MCTRL and MSTATUS reading is OK, completion bit is set correctly.

[00:24:52.345,217] <dbg> i3c_mcux: mcux_i3c_has_error: ERROR: MCTRL 0x0000d250 MSTATUS 0x00009403 MERRWARN 0x00100000

 

0 件の賞賛
返信
1,360件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Correction: I DON'T think bus will die if timeout bit is set. 

 

0 件の賞賛
返信
1,370件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @galenc 

I chcked the i3c source code from Zephyr https://github.com/zephyrproject-rtos/zephyr/blob/70f55bccf8af2866331f6fd84e05c600f4457704/drivers/i... 

These codes in this file which follow Apache-2.0 were contributed from freescale, intel, nxp. I may need a little time to check if I can find right person to deal with this. Also, you can use Zephyr community ( Discussions and Issues ), they will support you directly.

 

About this I3C question(emit, IBI), I would like to share common driver from NXP: 

https://github.com/nxp-mcuxpresso/mcux-sdk/blob/main/drivers/i3c/fsl_i3c.c#L690

 

0 件の賞賛
返信
1,494件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @galenc 

It seems some issues releated to I3C, Zephyr, lsm6dso sensor and SDK. I try to clairfy what I found one by one as below, hope these comments help you find the root cause.

 

1. It seems support wm8904 codec as default I3C in Zephyr

 https://github.com/zephyrproject-rtos/zephyr/blob/main/boards/nxp/mimxrt685_evk/mimxrt685_evk_mimxrt... 

https://github.com/zephyrproject-rtos/zephyr/blob/main/boards/nxp/mimxrt685_evk/mimxrt685_evk-pinctr... 

&i3c0 {
	pinctrl-0 = <&pinmux_i3c>;
	pinctrl-names = "default";

	status = "okay";

	audio_codec: wm8904@1a0000000000000000 {
		compatible = "wolfson,wm8904";
		reg = <0x1a 0 0>;

		clock-source = "MCLK";

		clocks = <&clkctl0 MCUX_AUDIO_MCLK>;
		clock-names = "mclk";
	};
};

 And actually I find it seems only support I2C(not mentioned I3C) from the introdcution https://github.com/zephyrproject-rtos/zephyr/blob/main/boards/nxp/mimxrt685_evk/doc/index.rst 

PIO0_17 I2C I2C SDA
PIO0_18 I2C I2C SCL

 

2. If you use EVKMIMXRT685, I would like to recommend you to use offical SDK instead for testing. Please note the necessary board setting of I3C before your quick start, https://github.com/nxp-mcuxpresso/mcux-sdk-examples/tree/main/evkmimxrt685/driver_examples/i3c/polli... 

 3. Also please check the sensor part(salve) independently whether this sensor support I3C or not.

4. Currently it is diffcult to give clear direction or sw/hw issue.

 

B.R,

Sam

0 件の賞賛
返信