RT685-AUD-EVK Can not get the record playback example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT685-AUD-EVK Can not get the record playback example

Jump to solution
2,803 Views
mrichardson23
Contributor IV

I can not get the TDM Record and Playback example to work.  I plug in my source and my output, but nothing plays.  When I check the buffers, I don't see anything except an occasional FF.  What am I doing wrong with this example?

Labels (1)
0 Kudos
Reply
1 Solution
2,636 Views
mrichardson23
Contributor IV

There was some kind of issue with the environment.  I got it working in xpresso and then tried again in vs code and it worked.  Not sure what was going on.

View solution in original post

0 Kudos
Reply
4 Replies
2,637 Views
mrichardson23
Contributor IV

There was some kind of issue with the environment.  I got it working in xpresso and then tried again in vs code and it worked.  Not sure what was going on.

0 Kudos
Reply
2,626 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @mrichardson23 ,

   Thanks for your updated information.

  So, it's working on your side now, right?

  When you meet the issues, you also can try to clean the project and build project again if you suspect the environment.

  If your question is solved, please help to mark the correct answer, just to close this case, thanks.

  Any new issues, welcome to create the new case.

Best Regards,

Kerry

0 Kudos
Reply
2,619 Views
mrichardson23
Contributor IV

Thanks @kerryzhou - not sure what to mark as the solution since there is no real answer to this but I will mark as solved.

0 Kudos
Reply
2,735 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @mrichardson23 ,

  Which code you are using now? SDK code?

 Please try the newest SDK:

\SDK_2_14_0_MIMXRT685-AUD-EVK\boards\mimxrt685audevk\driver_examples\i2s\dma_tdm_record_playback

Please also note the board configuration:

Hardware requirements
=====================
- Micro USB cable
- MIMXRT685-AUD-EVK board
- Personal Computer
- headphones with 3.5 mm stereo jack
- source of sound (line output to 3.5 mm stereo jack)
- Line in line

Board settings
==============
To make example work, please make sure board settings are applied:
JP43 1-2, R488 1-2
R479 1-2, R429 1-2
R480 1-2, R481 1-2
R510 1-2, R474 1-2
R482 1-2, R478 1-2
JP8 1-2, R491 1-2
R394 1-2, R395 1-2

Prepare the Demo
================
1. Connect headphones to J4 or J50 or J51 or J52.
2. Connect source of sound(from PC or Smart phone) to Audio Line-In connector (J56 or J55, J57).
3. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
4. Open a serial terminal with the following settings:
- 115200 baud rate
- 8 data bits
- No parity
- One stop bit
- No flow control
5. Download the program to the target board.
6. Launch the debugger in your IDE to begin running the demo.
Running the demo

 

if you still have issues, please kindly let me know.

Best Regards,

kerry

0 Kudos
Reply