RT600 I3C HDR mode support using i3c drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT600 I3C HDR mode support using i3c drivers

1,347 Views
aqeel21
Contributor I

Hello, I have got two RT600 boards, setup as one being the master and other the slave. I can communicate over the SDR mode using the provided examples(polling_b2b_transfer/master ) but i want to communicate over the HDR-DDR mode. I have changed the slave and master config and created a transfer message with HDR-DDR mode enabled. So. far i cannot see the messages being delivered over the slave and neither is the slave being able to reply back to master in the HDR mode. I wanted ask, if its supported and if i need to call some other functions to enable the HDR-DDR mode other then setting them up in the config and "Xfer" message. Thank-you for the support

0 Kudos
Reply
1 Reply

1,336 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

As for today, the i3c drivers that we provide within the SDK are very limited. We are aware that we are missing support of some key features of the I3C protocol. The SDK team is working on adding those in future releases of the SDK. Unfortunately, right now we don't have official support for HDR-DDR mode in our I3C drivers. I apologize for the inconvenience that this might cause you. 

Regards,
Victor 

0 Kudos
Reply