RT600 Getting Started error - Xtensa OCD Daemon: Target DLL not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT600 Getting Started error - Xtensa OCD Daemon: Target DLL not found

ソリューションへジャンプ
3,125件の閲覧回数
mhp
Contributor I

Hi, 

I'm trying to bring up the RT685 board for running DSP applications. I'm following the guide at: https://www.nxp.com/document/guide/getting-started-with-i-mx-rt600-evaluation-kit:GS-MIMXRT685-EVK#t...

I can successfully build and run the Arm application from MCUXpresso.

But get this error when running the Xtensa OCD Daemon application. 

mhp_0-1654164543454.png

I have confirmed that the serial number in the topology file matches that of the LPC-Link2.

When trying to run the jLink DLL updater no application are ready for update.

Hope someone can help me get it to work, please let me know if more information is needed.

 

Setup:

PC with Windows 10

MIMXRT685-EVK

MCUXpresso v11.5.1

Xtensa OCD Daemon v14.05

Xtensa Xplorer v8.0.15

 

Best Regards

Mikkel

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,121件の閲覧回数
mhp
Contributor I

Solved - Needed to run the command prompt as administrator.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,122件の閲覧回数
mhp
Contributor I

Solved - Needed to run the command prompt as administrator.

0 件の賞賛
返信