Hi,
First of all, it is necessary to list which masters are on the bus. Certainly CM7, CM4 and DMA are masters. What other masters are there?
USB has an internal DMA, right? So USB could be considered a master?
Does the same argument apply to ENET?
The TCM of CM4 is a slave on the bus right? Or not, since it communicates with the CM4 core via a dedicated bus?
In any case, the question is, which master can access CM4's TCM?
best regards
Max