RT117x how to use GUI_guider V1.2 build file system support hmi project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT117x how to use GUI_guider V1.2 build file system support hmi project

Jump to solution
1,348 Views
ClusterDesign
Contributor I

Dear Support:

    Recently we use GUI_Guider V1.2 building HMI project based on RT1170 EVK board. Unfortunately, i can not find the file system supporting settings on that tool. Each picture generate a .c source code. That's impossible for us to use this tool to create a project with nearly 1000 pictures in .c code. I wish to know how can i use GUI_guider to create a HMI project can split picture & font using file system to store the file in flash or eMMC not using .c files. 

0 Kudos
Reply
1 Solution
1,324 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ClusterDesign,

This question has been addressed on the following thread. I'm including the link in case it helps other community users with the same question.

https://community.nxp.com/t5/GUI-Guider/How-to-use-GUI-guider-V1-2-build-file-system-support-hmi-pro...

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
2 Replies
1,325 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ClusterDesign,

This question has been addressed on the following thread. I'm including the link in case it helps other community users with the same question.

https://community.nxp.com/t5/GUI-Guider/How-to-use-GUI-guider-V1-2-build-file-system-support-hmi-pro...

Regards,
Gustavo

0 Kudos
Reply
1,319 Views
ClusterDesign
Contributor I

Hi Gustavo:

    Thanks for your information.

Best Regards,

0 Kudos
Reply