RT117x With TJA1103 or TJA1120 with 3.3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT117x With TJA1103 or TJA1120 with 3.3V

Jump to solution
785 Views
Wobaffet
Senior Contributor I

Hello, 

We want to use TJA1103A or TJA1120A with RT117x Crossover MCU in RGMII mode. On the EVK, it is driven with 1.8V so is it possible to use these ICs on 3.3V without any performance or feature compromise?

MicrosoftTeams-image.png

Thank you in advance!

Best Regards.

0 Kudos
Reply
1 Solution
770 Views
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @Wobaffet 

 

Thanks a lot for reaching our technical support and for your patience.

 

Regarding your question, yes, you can use it with 3.3V too, as the schematic from the EVK shows both options. Regarding "performance or feature compromise", it shouldn't be anything.

 

Hope that helps you.

 

BR.

Pablo Avalos.

View solution in original post

1 Reply
771 Views
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @Wobaffet 

 

Thanks a lot for reaching our technical support and for your patience.

 

Regarding your question, yes, you can use it with 3.3V too, as the schematic from the EVK shows both options. Regarding "performance or feature compromise", it shouldn't be anything.

 

Hope that helps you.

 

BR.

Pablo Avalos.