Hi @rubensjunior ,
I have identified some pins for the ENET 1G Ethernet Controller. You can verify these in the Pin Configuration tool. These pins offer multiple functionalities, and I found the following features for the 1G Ethernet:
- RGMII/RMII/MII operation
- Support for IEEE1588
- Support for AVB
The required pins for Ethernet are mentioned in the Pin Configuration tool. Please match the Ethernet pins from the tool with the pin mapping table I am sharing here.
Note: I have not tested these pins; the pin mapping design is as per the MCU Expresso Config Tool.
I hope this will be helpful to you.
Additionally, @EdwinHz, could you please guide this suggestion?
Pin Mapping Table:
| ENET_TXD0 | ENET_TX_DATA_0 (E9) | ENET_TXD0 | GPIO_DISP_B2_02 | E9 |
| ENET_TXD1 | ENET_TX_DATA_1 (D7) | ENET_TXD1 | GPIO_DISP_B2_03 | D7 |
| ENET_TXEN | ENET_TX_EN (C7) | ENET_TXEN | GPIO_DISP_B2_04 | C7 |
| ENET_RXD0 | ENET_RX_DATA_0 (C6) | ENET_RXD0 | GPIO_DISP_B2_06 | C6 |
| ENET_RXD1 | ENET_RX_DATA_1 (D6) | ENET_RXD1 | GPIO_DISP_B2_07 | D6 |
| ENET_CRS_DV | ENET_RX_EN (B5) | ENET_CRS_DV | GPIO_DISP_B2_08 | B5 |
| ENET_RXER | ENET_RX_ER (D8) | ENET_RXER | GPIO_DISP_B2_09 | D8 |
| ENET_RST | GPIO8_IO27 (T2) | ENET_RST | GPIO_EMC_B2_17 | T2 |
| ENET_MDC | ENET_MDC (U2) | ENET_MDC | GPIO_EMC_B2_19 | U2 |
| ENET_MDIO | ENET_MDIO (R3) | ENET_MDIO | GPIO_EMC_B2_20 | R3 |
| ENET_INT | GPIO13_IO08 (P9) | ENET_INT | GPIO_SNVS_05 | P9 |
Thanks
Sagar