RT1176 SEMC SDRAM sdramconfig.tPrescalePeriod_Ns value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 SEMC SDRAM sdramconfig.tPrescalePeriod_Ns value

Jump to solution
877 Views
Boscfab
Contributor I

Hi everyone,
I'm trying to configure the parameters of the SEMC for my SDRAM bank with RT1176.
In the various parameters, in the EVB settings the value
"sdramconfig.tPrescalePeriod_Ns" it's "160 * (1000000000 / clockFrq)".

NOTE: EVB use 2x16bit SDRAM mod.W9825G6KH-5I with CLK=200MHz.

I use different SDRAM chips with 166MHz CLOCK but I don't know what data must be use to calculate this parameter; I have configured all the other parameters correctly but I don't understand this.
Does anyone know how to configure this parameter or can point me to an APPNOTE that describes it.

Thank you,

 

Fabio

0 Kudos
Reply
1 Solution
856 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Prescaler period is used as a clock cycle count unit for refresh and bus idle timer period. Please refer to this example:

Omar_Anguiano_0-1685648666578.png

Best regards,
Omar

View solution in original post

0 Kudos
Reply
2 Replies
857 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Prescaler period is used as a clock cycle count unit for refresh and bus idle timer period. Please refer to this example:

Omar_Anguiano_0-1685648666578.png

Best regards,
Omar

0 Kudos
Reply
812 Views
Boscfab
Contributor I

Perfect, the answer is exhaustive!
Is there a SEMC controller AppNote that describes how to optimize the setup of the various parameters?

The RT117xx family data sheet does not contain these useful explanations....

 

Many Thanks,

 

Fabio

0 Kudos
Reply