mdk keil (RT1176 EVK):
when i select the flexspi_nor_sdram release project,after i rebuild it and load to the rt1176,evk board can not run well (just like dead crash),the same with putting the reset button;
when i select the flexspi_nor_sdram debug project,after i rebuild it and load to the rt1176,evk board can run well(debug run and then stoped the debug window),but when i putting the reset button;the evk board crashed;
i try to using the secure provising tool to connect the evk board but always failed(through the sdp usb port, tip: boot mode (both 00 and 01 all used to try))
that‘s why, thanks for your help
Best Regards!
Hello,
If you are doing all ok the is probably that you have a damage board, please contact your vendor for this reason.
Regards