RT1176 更换SDRAM大小后官方SDCARD例程无法正常运行

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 更换SDRAM大小后官方SDCARD例程无法正常运行

1,569 Views
demoncui
Contributor I

你好:

     我们有个项目采用的是RT1176,最初是用的256Mb的SDRAM,最近更换为pin to pin的同厂商的128Mb的SDRAM后有些功能就无法正常使用。从官网上下载sdcard_fatfs_cm7(版本为2.11.1,工具为KEIL,用的sdcard_fatfs_cm7 flexspi_nor_release工程)例程,使用256Mb的SDRAM硬件SD卡可以正常读写操作,更换为128Mb的SDRAM后程序可跑,但是SD卡无法识别,跟SD有关的例程都是SD那部分无法正常工作。求助可能原因。

1,官方的例程中关于SDRAM的大小都是设置的64M?

2 ,在sdcard_fatfs_cm7 flexspi_nor_release模板下未找到SDRAM设置的地方,分散加载文件中也未看到有SDRAM的描述。

求助是否是需要更改哪些配置

0 Kudos
Reply
2 Replies

1,535 Views
demoncui
Contributor I

谢谢回复。我试了几个关于SD的例程,我核心板将256的换成128的内存后SD卡部分就不正常了,我再找找原因

0 Kudos
Reply

1,552 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @demoncui ,

1.是的SDK里的例程是64M SDRAM。因为所有例程都是基于EVK。

2.是的,这个例程没有用到SDRAM。你可以看到没有定义XIP_BOOT_HEADER_DCD_ENABLE。

 

Regards,

Jing

0 Kudos
Reply