RT1170 evkb does not boot(QSPI, hello word example)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 evkb does not boot(QSPI, hello word example)

Jump to solution
840 Views
yudoc
Contributor I

Hi, I just opened the EVK box and tested it.
I compiled one of the examples called `hello_world_demo_cm7` and it does not work. I also tried a couple of other examples, but it still does not work. the SDK version is 2.16

 

Screenshot from 2024-11-04 09-56-20.png


After finishing downloading the firmware, it gets stuck here. 

I also tried to execute the same code on the Sram, it was working fine.  

Is there anything I can do?

 

0 Kudos
Reply
1 Solution
812 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @yudoc,

There are two EVK for RT1170, EVK and EVKB, each one has his respective SDK.

Pablo_Ramos_0-1730746325646.png

Could you check if the EVK you have match with the SDK you are using?

Please let me know your results

View solution in original post

1 Reply
813 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @yudoc,

There are two EVK for RT1170, EVK and EVKB, each one has his respective SDK.

Pablo_Ramos_0-1730746325646.png

Could you check if the EVK you have match with the SDK you are using?

Please let me know your results