I want to debug the official TSN demo,but the demo must build in ubuntu environment,Is there a demo that can run on MCU Expresso ide or keil?
Hi @kerryzhou ,
I have made two RT1176 boards refered to RT1176 EVK NXP, but I found they can't transmit message.My log showed too much errflow ,and err frames is as many as tx frames,like this q1 tx: 476603, err: 346192,I was so confused about it .Do you know what's the meaning of socket_stats_print and how link it up? My stats_print always shows link down! My log showed in attachment. Thank you very much!
Hi @HanaYu
If you have any questions, could you please create your own question post?
In your own question post, tell us which detail code you are using, and whether you modify the code, and the code source is from NXP or not, if from NXP, also share the link, then we can help you in your own question post directly, thanks.
Best Regards,
Kerry
Hi @IvyGuo ,
I checked internally, still just linux version, no windows version.
But have the mcuxpresso version, please check this one:
You will get genavb_tsn-mcuxpresso-SDK_2_10_0-4_0_3.zip
Wish it helps you!
Best Regards,
kerry
Hi,Kerry!
Thanks for your reply,I download the zip file,I found no project file when i used the linux version mcu expresso ide to import the project,how to import the full tsn sdk into linux version mcu expresso ide?
I wonder how to debug when the nxp develop the tsn demo? just use printf funtion into project to monitor the error? Please kindly help to solve the issue,thank you.
Hi @IvyGuo ,
I help you check the internal side, as the TSN is designed based on the linux, so still no windows method.
About the detail usage, each package contains the doc document, you can read the related document, eg:
genavb_tsn-mcuxpresso-SDK_2_10_0-4_0_3\doc
some Chinese document also useful to you:
https://mp.weixin.qq.com/s/qOckDro-ROKgBlbL8-Jj1Q
https://mp.weixin.qq.com/s/UYl6DDYIQCA8Ne6kANEk7w
Wish it helps you!
Best Regards,
Kerry
Dear,Kerry!
Thanks for your reply,I'd like to know if I want to verify the QBU feature of the TSN Demo,two endpoint devices must RT1170-EVK? One board can not test qbu feature? can not capture the key frame? Do you have any suggestion?
Hi @IvyGuo ,
As still no other PC side tool to act as another point to test it, so maybe still need two EVK boards to test QBU feature.
Best Regards,
Kerry