RT1170 SEMC Wait duration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 SEMC Wait duration

Jump to solution
1,779 Views
Eugene3
Contributor II

I'm designing an RT1170-based design that will interface with SRAM via the SEMC peripheral.

The SRAM is asynchronous thus I plan to use wait pin.

Are there any spec for wait assertion duration? I'd like to know the maximum wait time allowed.

0 Kudos
Reply
1 Solution
1,745 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi  @Eugene3 ,

 

No, RT1170 doesn't have such kind of timeout event, but the Wait Valid Time must be no less than 2 semc_clk cycles. Please check the data sheet of your SRAM device for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,764 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 

Actually the WAIT signal is a signal from the SRAM side, the duration is not controlled by RT1170 indeed. 

Please kindly refer to the following for more details.

Kan_Li_0-1698827463096.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
1,756 Views
Eugene3
Contributor II

Hi @Kan_Li 

Thank you for your replying.

If SRAM device assert wait signal so long time, does RT1170 have a timeout? 

0 Kudos
Reply
1,746 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi  @Eugene3 ,

 

No, RT1170 doesn't have such kind of timeout event, but the Wait Valid Time must be no less than 2 semc_clk cycles. Please check the data sheet of your SRAM device for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,742 Views
Eugene3
Contributor II

Hi @Kan_Li 

Thank you for your help. 

0 Kudos
Reply