[RT1170] [LPADC] ADC sample project problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RT1170] [LPADC] ADC sample project problem

Jump to solution
2,315 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello ,All

 

I am testing the LPADC sample project for customer.

As Readme shows that the ADC can convert each value for J9-10 and J9-16,.

As far as I have measured ,

But  J9-16 value is always same as that of J9-10(Input voltage to J9-16 is different from J9-10) and can not detect the voltage well.

ZHOU_XIAO_0-1654480237241.png

The J9-10 can detect the value well.

Could you confirm this sample code? Our evaluation condition is as below. [Board] SDK_2.x_MIMXRT1170-EVK [SDK] SDK Version 2.11.1 [Sample Code] driver_examples\adc_etc\adc_etc_hardware_trigger_conv\cm7\lpadc_etc_hardware_trigger_conv.c

 

Best Regards

ZHOU

0 Kudos
Reply
1 Solution
2,285 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello,kerry ZHOU

 

Albort xue has already created a ticket to trace/follow this problem . He told me that the fixed one will be release in SDK 2.12.1.

 

Best regards

ZHOU

View solution in original post

0 Kudos
Reply
4 Replies
2,296 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ZHOU_XIAO ,

   We are NXP colleague!

   In fact, if you have any issues, you can create the internal question post here in stead of the public community:

https://community.nxp.com/t5/RT-4-Digit-10xx-11xx-12xx/gh-p/52590

  Then our AE can help us directly.

   To your question, do you connect the J9-10 and J9-16 to the same fixed voltage, which voltage point in the MIMXRT1170-EVK board? About the connection, you also need to make sure the wire connection is good!

  Then, I will assign time to test it.

  If we find any issues, we also can report to our SDK team directly.

Best Regards,

Kerry

0 Kudos
Reply
2,291 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello,@jerryzhou

 

SDK team member Albort XUE has already sent me the modified C source file to me and

after replacing the C file source, it turns to work well now.

 

Sorry to post this problem in public community , I will post in internal community next time.

 

Best regards

ZHOU

0 Kudos
Reply
2,288 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ZHOU_XIAO ,

   Thanks for the updated information, so it is confirmed the SDK bug, and internal side already report it, right?

   As our new SDK will be published in the near future, so, it's better to report to the SDK team to fix it, thanks.

Best Regards,

kerry

0 Kudos
Reply
2,286 Views
ZHOU_XIAO
NXP Employee
NXP Employee

Hello,kerry ZHOU

 

Albort xue has already created a ticket to trace/follow this problem . He told me that the fixed one will be release in SDK 2.12.1.

 

Best regards

ZHOU

0 Kudos
Reply