RT1170-EVK ADC_ETC target commandID setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170-EVK ADC_ETC target commandID setting

636件の閲覧回数
auftrag2021
Contributor III

Hello 

HW: RT1170EVK

SW: MCUXpresso v11.5.0

I am trying to deep understand the LPADC and ADC_ETC configuration, here is one thing which I feel very strange

 

the LPADC setup was

auftrag2021_1-1646869292312.png

beside, the ADC_ETC setup was:

auftrag2021_2-1646869362692.png

The interesting thing is, I tested the example code with both scenarios, which means:

scenario 1: ADC target command ID = 1 (meanwhile LPADC command ID  = 1)

scenario 2: ADC target command ID = 2 (meanwhile LPADC command ID  = 1)

I was astonished, with different setting of this parameter, I always got the same result. Which means, the ADC give me always the same value from analog input channel which I set it up in LPADC1

It seems, the origin command ID = 1 from LPADC setup was "replaced" by the ADC_ETC (target command ID) setting. but why?

 

 

 

0 件の賞賛
返信
1 返信

624件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @auftrag2021 

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the application note.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信