Hi,
Both boards RT1160/RT1170 has mention in the user manual that they have CAN support, with already mounted drivers TJA1057
But I cant find where they are.
Where the CAN can be connected at these boards?
Thanks
Solved! Go to Solution.
Hi @temmka
The boards come with 3 simple 2.5 mm holes that are described as CAN Bus Connector for CANL, CANH and GND. You need to solder pins or a cables to them. There is no DB9 connector on i.MX RT EVKs.
In RT1160-EVK this is J47.
I wish this hepls you!
Diego
Hi @temmka
The boards come with 3 simple 2.5 mm holes that are described as CAN Bus Connector for CANL, CANH and GND. You need to solder pins or a cables to them. There is no DB9 connector on i.MX RT EVKs.
In RT1160-EVK this is J47.
I wish this hepls you!
Diego