RT1160/RT1170 CAN-BUS connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1160/RT1170 CAN-BUS connection

Jump to solution
718 Views
temmka
Contributor II

Hi, 
Both boards RT1160/RT1170 has mention in the user manual that they have CAN support, with already mounted drivers TJA1057

temmka_0-1709163716341.png

But I cant find where they are.

Where the CAN can be connected at these boards?

Thanks

0 Kudos
Reply
1 Solution
682 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @temmka 

The boards come with  3 simple 2.5 mm holes that are described as  CAN Bus Connector for CANL, CANH and GND. You need to solder pins or a cables to them. There is no DB9 connector on i.MX RT EVKs.

In RT1160-EVK this is J47.

diego_charles_0-1709663832221.png

diego_charles_1-1709664030569.png

I wish this hepls you!

Diego

 

 

 

 

View solution in original post

2 Replies
683 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @temmka 

The boards come with  3 simple 2.5 mm holes that are described as  CAN Bus Connector for CANL, CANH and GND. You need to solder pins or a cables to them. There is no DB9 connector on i.MX RT EVKs.

In RT1160-EVK this is J47.

diego_charles_0-1709663832221.png

diego_charles_1-1709664030569.png

I wish this hepls you!

Diego

 

 

 

 

676 Views
temmka
Contributor II
Thank you Diego!
0 Kudos
Reply