RT1160 Dual Image support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1160 Dual Image support

Jump to solution
1,178 Views
iann
Contributor III

Hi for the application we're developing using the MIMXRT1166 we're looking at whether the internal boot ROM is enough to handle our program updates in the field. The Dual image support sounds very useful but there isn't much information apart from 10.13.3 Enter Bootloader API in the Reference Manual

Enter bootloader.png

but it isn't mentioned again.

Are there further app notes or SDK examples where this is elaborated on?

I found some more information in the IMXRT1170RM 

Dual image IMXRT1170.png

Does this also apply to the RT1160 parts?

Thanks for any help

Ian Norman

0 Kudos
Reply
1 Solution
1,136 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @iann 

Yes, dual image support should also apply for RT1160.

Currently, we have this document Pi Ziheng Embedded: Revealing the alternate boot design of serial NOR Flash dual programs on i.MXRT1... . This article was written  by a chinese colleague, in chinese, please translate it to english. 

I hope this could help you. 

Diego

View solution in original post

0 Kudos
Reply
5 Replies
1,137 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @iann 

Yes, dual image support should also apply for RT1160.

Currently, we have this document Pi Ziheng Embedded: Revealing the alternate boot design of serial NOR Flash dual programs on i.MXRT1... . This article was written  by a chinese colleague, in chinese, please translate it to english. 

I hope this could help you. 

Diego

0 Kudos
Reply
613 Views
Littell
Contributor III

It is so unbelievably ridiculous that proper documentation in English can't be provided for these devices.  You guys (NXP) really need to get your act together.

0 Kudos
Reply
595 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Littell 

I understand the frustration, at this time, and currently,  the Chinese article was the only documentation available for this topic. We are currently working on delivering further documentation on this topic. We require to align with bootROM development team to create official documentation, as for other documents and this migth require more time, than the expected. 

If you need any assistance with this topic, feel free to let me know. I have a draft article about setting RT1170 and dual image testing with the Secure Provisioning Tool. I can share the steps  you, and if you have any additional feedback that could be helpful. 

Thank you very much for your interest!

Diego

 

 

0 Kudos
Reply
588 Views
Littell
Contributor III

4 months for better documentation on a topic that appears to be driving a number of people in this forum crazy?  I'll take any information I can get, though, it's not likely to be any worse than what's out there already.  I'll start a new thread "RT1170 dual image support wi/ROM API's explained for real" and let's see where it goes.

What a nightmare.

0 Kudos
Reply
1,125 Views
iann
Contributor III
Thank you very much for confirming, and the extra document is very helpful.

Ian