Hello team,
My customer looking to capture and store video/movie using the mipi-csi camera interface at 10 fps with a maximum resolution of camera 720P (10 fps).
1. Please advise if iMXRT1160 oriMXRT1170 support the above requirement ?
2. Also they plan to compress the video (after storing it on an SD card), please advise back what is the best compression method in the RT1160/70?
Waiting for your kind feedback, many thanks.
Best Regards,
Shai
Hello
I hope you are well.
Maximal resolution for MIPI-CSI is 65 535 x 65 535 pixels and the maximum throughput is 75Mpix/s peak.
So, yes that resolution is supported.
Regarding the compression method, it will depend on your project requirements so I cannot give a specific recommendation.
However, I suggest you check H.264 since we already have an application note for reference: AN13205: Development of H.264 Video Encode on i.MX RT Series – Application Note (nxp.com)
Best regards,
Omar