I have an application that requires booting from the qspi to SDRAM. I got that to work by setting the plain load checkbox in mcuexpresso, making the SDRAM start at 0x80002000 and modifying the Boot Data structure (BOOT_DATA_T in the fsl_flexspi_nor_boot.c file) to have a start location of 0x80002000, so that the image can be loaded straight to sdram including all the headers. This works fine and i can use the debugger in attach only mode. However it is annoying to first load the image into flash with the GUI Flash tool in the debug configuration. When i debug directly i get execution at some bogus address, i think it's because the debugger tries to stop early or something. How would i set this up so that i can have a one click workflow?
Thanks in advance,
Konstantin