RT106x crystal drive level spec requirement.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT106x crystal drive level spec requirement.

1,019 Views
StephenYeh
Contributor III

Would you share the RT106x EVK crystal part number?

And we check the spec. crystal drive level is 250uW.

If we choose crystal spec max 100uW, it will damage by RT106x.

Or just choose below DL 250uW will be OK? 

0 Kudos
Reply
3 Replies

1,013 Views
StephenYeh
Contributor III

Hi Jeremy

Thank for your quickly reply.

Sorry, Where the BOM file I could download?

0 Kudos
Reply

1,011 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Attachment may show up later after virus scanning completes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,015 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Would you share the RT106x EVK crystal part number?
-- I've attached the BOM file, please check its part number.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply