RT1064+Jlink debug issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1064+Jlink debug issue

跳至解决方案
8,996 次查看
colinluan
Contributor III

Hello,

My jlink suddenly couldn't connect to my RT1064 board, and now the J-link commander only can get the RT1064 information but cannot debug in MCUXPresso. 

My debug environment: 

IDE

CUXPresso 10.3.1

Debuger

Jlink Base

Debuger Driver

Jlink V6.84 Driver

 

1. The J-Link Commander can get the RT1064 information

1064-detect.png

2. MUCXPresso shows following error

0xdeadbeee.png

and the jlink display following log:

 

 

 

SEGGER J-Link GDB Server V6.84 GUI Version

JLinkARM.dll V6.84 (DLL compiled Sep  4 2020 16:12:50)

-----GDB Server start settings-----
GDBInit file:                  none
GDB Server Listening port:     2331
SWO raw output listening port: 2332
Terminal I/O port:             2333
Accept remote connection:      localhost only
Generate logfile:              off
Verify download:               on
Init regs on start:            off
Silent mode:                   off
Single run mode:               on
Target connection timeout:     5000 ms
------J-Link related settings------
J-Link Host interface:         USB
J-Link script:                 none
J-Link settings file:          none
------Target related settings------
Target device:                 MIMXRT1064DVL6A
Target interface:              SWD
Target interface speed:        1000kHz
Target endian:                 little

Connecting to J-Link...
J-Link is connected.
Device "MIMXRT1064XXX6A" selected.
Firmware: J-Link V10 compiled Jul 17 2020 16:23:38
Hardware: V10.10
S/N: 50124254
Feature(s): GDB
Checking target voltage...
Target voltage: 3.35 V
Listening on TCP/IP port 2331
Connecting to target...
InitTarget() start
InitTarget()
_TargetHalt: CPU halted
InitTarget() end
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 2 bytes @ address 0x7003B540 (Data = 0xFFFF)
Read 2 bytes @ address 0x7002FB50 (Data = 0x7372)
Read 4 bytes @ address 0x70029CAC (Data = 0x3102E7FE)
Reading 64 bytes @ address 0x20200E80
Read 4 bytes @ address 0x700039DA (Data = 0xF503687B)
Reading 64 bytes @ address 0x20200E40
Reading 8 bytes @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
Reading 8 bytes @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
WARNING: Failed to read memory @ address 0xB8400000
Received monitor command: reset
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Resetting target
Downloading 8192 bytes @ address 0x70000000 - Verified OK
Downloading 16144 bytes @ address 0x70002000 - Verified OK
Downloading 15744 bytes @ address 0x70005F10 - Verified OK
Downloading 16128 bytes @ address 0x70009C90 - Verified OK
Downloading 16032 bytes @ address 0x7000DB90 - Verified OK
Downloading 16144 bytes @ address 0x70011A30 - Verified OK
Downloading 16144 bytes @ address 0x70015940 - Verified OK
Downloading 16128 bytes @ address 0x70019850 - Verified OK
Downloading 16128 bytes @ address 0x7001D750 - Verified OK
Downloading 16192 bytes @ address 0x70021650 - Verified OK
Downloading 16096 bytes @ address 0x70025590 - Verified OK
Downloading 16112 bytes @ address 0x70029470 - Verified OK
Downloading 16096 bytes @ address 0x7002D360 - Verified OK
Downloading 16096 bytes @ address 0x70031240 - Verified OK
Downloading 16144 bytes @ address 0x70035120 - Verified OK
Downloading 16192 bytes @ address 0x70039030 - Verified OK
Downloading 16320 bytes @ address 0x7003CF70 - Verified OK
Downloading 15000 bytes @ address 0x70040F30 - Verified OK
Downloading 2956 bytes @ address 0x700449C8 - Verified OK
Downloading 2360 bytes @ address 0x70045554 - Verified OK
Downloading 1748 bytes @ address 0x70045E8C - Verified OK
Downloading 3600 bytes @ address 0x70046560 - Verified OK
ERROR: Failed to download RAMCode.
Failed to prepare for programming.
Failed to download RAMCode!
Writing register (PC = 0x700022f4)
Read 2 bytes @ address 0x7003B540 (Data = 0x31BF)
Read 2 bytes @ address 0x7002FB50 (Data = 0x31BF)
Read 2 bytes @ address 0x7003B540 (Data = 0x31BF)
Read 2 bytes @ address 0x7002FB50 (Data = 0x31BF)
Reading all registers
WARNING: Failed to read memory @ address 0xFFFFFFFE
Reading 64 bytes @ address 0x7002F200
Read 2 bytes @ address 0x7002F220 (Data = 0x31BF)
Received monitor command: semihosting enable
Semi-hosting enabled (Handle on BKPT)
Received monitor command: exec SetRestartOnClose=1
Executed SetRestartOnClose=1
Received monitor command: reset
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Resetting target
Setting breakpoint @ address 0x7002F220, Size = 2, BPHandle = 0x0001
Starting target CPU...
ERROR: Could not start CPU core. (ErrorCode: -1)
ERROR: Cannot read register 15 (R15) while CPU is running
Reading all registers
ERROR: Cannot read register 0 (R0) while CPU is running
ERROR: Cannot read register 1 (R1) while CPU is running
ERROR: Cannot read register 2 (R2) while CPU is running
ERROR: Cannot read register 3 (R3) while CPU is running
ERROR: Cannot read register 4 (R4) while CPU is running
ERROR: Cannot read register 5 (R5) while CPU is running
ERROR: Cannot read register 6 (R6) while CPU is running
ERROR: Cannot read register 7 (R7) while CPU is running
ERROR: Cannot read register 8 (R8) while CPU is running
ERROR: Cannot read register 9 (R9) while CPU is running
ERROR: Cannot read register 10 (R10) while CPU is running
ERROR: Cannot read register 11 (R11) while CPU is running
ERROR: Cannot read register 12 (R12) while CPU is running
ERROR: Cannot read register 13 (R13) while CPU is running
ERROR: Cannot read register 14 (R14) while CPU is running
ERROR: Cannot read register 15 (R15) while CPU is running
ERROR: Cannot read register 16 (XPSR) while CPU is running
ERROR: Cannot read register 17 (MSP) while CPU is running
ERROR: Cannot read register 18 (PSP) while CPU is running
ERROR: Cannot read register 24 (PRIMASK) while CPU is running
ERROR: Cannot read register 25 (BASEPRI) while CPU is running
ERROR: Cannot read register 26 (FAULTMASK) while CPU is running
ERROR: Cannot read register 27 (CONTROL) while CPU is running
ERROR: Cannot read register 32 (FPSCR) while CPU is running
ERROR: Cannot read register 33 (FPS0) while CPU is running
ERROR: Cannot read register 34 (FPS1) while CPU is running
ERROR: Cannot read register 35 (FPS2) while CPU is running
ERROR: Cannot read register 36 (FPS3) while CPU is running
ERROR: Cannot read register 37 (FPS4) while CPU is running
ERROR: Cannot read register 38 (FPS5) while CPU is running
ERROR: Cannot read register 39 (FPS6) while CPU is running
ERROR: Cannot read register 40 (FPS7) while CPU is running
ERROR: Cannot read register 41 (FPS8) while CPU is running
ERROR: Cannot read register 42 (FPS9) while CPU is running
ERROR: Cannot read register 43 (FPS10) while CPU is running
ERROR: Cannot read register 44 (FPS11) while CPU is running
ERROR: Cannot read register 45 (FPS12) while CPU is running
ERROR: Cannot read register 46 (FPS13) while CPU is running
ERROR: Cannot read register 47 (FPS14) while CPU is running
ERROR: Cannot read register 48 (FPS15) while CPU is running
ERROR: Cannot read register 49 (FPS16) while CPU is running
ERROR: Cannot read register 50 (FPS17) while CPU is running
ERROR: Cannot read register 51 (FPS18) while CPU is running
ERROR: Cannot read register 52 (FPS19) while CPU is running
ERROR: Cannot read register 53 (FPS20) while CPU is running
ERROR: Cannot read register 54 (FPS21) while CPU is running
ERROR: Cannot read register 55 (FPS22) while CPU is running
ERROR: Cannot read register 56 (FPS23) while CPU is running
ERROR: Cannot read register 57 (FPS24) while CPU is running
ERROR: Cannot read register 58 (FPS25) while CPU is running
ERROR: Cannot read register 59 (FPS26) while CPU is running
ERROR: Cannot read register 60 (FPS27) while CPU is running
ERROR: Cannot read register 61 (FPS28) while CPU is running
ERROR: Cannot read register 62 (FPS29) while CPU is running
ERROR: Cannot read register 63 (FPS30) while CPU is running
ERROR: Cannot read register 64 (FPS31) while CPU is running
ERROR: Cannot read register 33 (FPS0) while CPU is running
ERROR: Cannot read register 34 (FPS1) while CPU is running
ERROR: Cannot read register 35 (FPS2) while CPU is running
ERROR: Cannot read register 36 (FPS3) while CPU is running
ERROR: Cannot read register 37 (FPS4) while CPU is running
ERROR: Cannot read register 38 (FPS5) while CPU is running
ERROR: Cannot read register 39 (FPS6) while CPU is running
ERROR: Cannot read register 40 (FPS7) while CPU is running
ERROR: Cannot read register 41 (FPS8) while CPU is running
ERROR: Cannot read register 42 (FPS9) while CPU is running
ERROR: Cannot read register 43 (FPS10) while CPU is running
ERROR: Cannot read register 44 (FPS11) while CPU is running
ERROR: Cannot read register 45 (FPS12) while CPU is running
ERROR: Cannot read register 46 (FPS13) while CPU is running
ERROR: Cannot read register 47 (FPS14) while CPU is running
ERROR: Cannot read register 48 (FPS15) while CPU is running
ERROR: Cannot read register 49 (FPS16) while CPU is running
ERROR: Cannot read register 50 (FPS17) while CPU is running
ERROR: Cannot read register 51 (FPS18) while CPU is running
ERROR: Cannot read register 52 (FPS19) while CPU is running
ERROR: Cannot read register 53 (FPS20) while CPU i

 

 

 

 

3. My jlink configuration

jlink-configure1.png

jlink-configure2.png.

Anybody has ever get this issue and give me some helps? thanks.

0 项奖励
回复
1 解答
8,970 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi colin,

Normally, this kind of problem is caused by application code has error and the core go into a unknow status. Please try to use MCUBootUtility to clear flash. You can download it from https://github.com/JayHeng/NXP-MCUBootUtility.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
2 回复数
8,971 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi colin,

Normally, this kind of problem is caused by application code has error and the core go into a unknow status. Please try to use MCUBootUtility to clear flash. You can download it from https://github.com/JayHeng/NXP-MCUBootUtility.

 

Regards,

Jing

0 项奖励
回复
8,956 次查看
colinluan
Contributor III

Thank you for your help, I have resolved this issue by switching to serial download mode and clear all flash, then I can debug after switching to internal mode.

0 项奖励
回复