RT1064 EVK Flashloader example removed from SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 EVK Flashloader example removed from SDK?

Jump to solution
1,760 Views
p_shep
Contributor IV

Hello,

I'm looking to build the example flashloader project for the RT1064... but I can't find it.

In the SDK 2.9.1 (and 2.9.0) there's some source code in .\middleware\mcu-boot, but I'm not sure how that fits into to a project. I could probably work it out, but I suspect there are example projects already available somewhere!

I have found the flashloader binary for the RT1064, but want to change a few things around for our purposes.

In RT1050 SDK there is the example flashloader project which I guess can be ported, but wonder if that might be older code.

So, where can I find the example flashloader project for the RT1064-EVK?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,757 Views
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

View solution in original post

0 Kudos
Reply
2 Replies
1,756 Views
p_shep
Contributor IV

Oh, but it doesn't include CAN. That's only available in the binary?

0 Kudos
Reply
1,758 Views
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

0 Kudos
Reply