RT1064 EVK Flashloader example removed from SDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064 EVK Flashloader example removed from SDK?

ソリューションへジャンプ
1,691件の閲覧回数
p_shep
Contributor IV

Hello,

I'm looking to build the example flashloader project for the RT1064... but I can't find it.

In the SDK 2.9.1 (and 2.9.0) there's some source code in .\middleware\mcu-boot, but I'm not sure how that fits into to a project. I could probably work it out, but I suspect there are example projects already available somewhere!

I have found the flashloader binary for the RT1064, but want to change a few things around for our purposes.

In RT1050 SDK there is the example flashloader project which I guess can be ported, but wonder if that might be older code.

So, where can I find the example flashloader project for the RT1064-EVK?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,688件の閲覧回数
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,687件の閲覧回数
p_shep
Contributor IV

Oh, but it doesn't include CAN. That's only available in the binary?

0 件の賞賛
返信
1,689件の閲覧回数
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

0 件の賞賛
返信