RT1064 EVK Flashloader example removed from SDK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1064 EVK Flashloader example removed from SDK?

跳至解决方案
1,683 次查看
p_shep
Contributor IV

Hello,

I'm looking to build the example flashloader project for the RT1064... but I can't find it.

In the SDK 2.9.1 (and 2.9.0) there's some source code in .\middleware\mcu-boot, but I'm not sure how that fits into to a project. I could probably work it out, but I suspect there are example projects already available somewhere!

I have found the flashloader binary for the RT1064, but want to change a few things around for our purposes.

In RT1050 SDK there is the example flashloader project which I guess can be ported, but wonder if that might be older code.

So, where can I find the example flashloader project for the RT1064-EVK?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,680 次查看
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,679 次查看
p_shep
Contributor IV

Oh, but it doesn't include CAN. That's only available in the binary?

0 项奖励
回复
1,681 次查看
p_shep
Contributor IV

Ah, so the magic is to select the USB host option on the SDK middleware components... ???

Now it's in the SDK build.

0 项奖励
回复