Hello,
I'm looking to build the example flashloader project for the RT1064... but I can't find it.
In the SDK 2.9.1 (and 2.9.0) there's some source code in .\middleware\mcu-boot, but I'm not sure how that fits into to a project. I could probably work it out, but I suspect there are example projects already available somewhere!
I have found the flashloader binary for the RT1064, but want to change a few things around for our purposes.
In RT1050 SDK there is the example flashloader project which I guess can be ported, but wonder if that might be older code.
So, where can I find the example flashloader project for the RT1064-EVK?
解決済! 解決策の投稿を見る。
Ah, so the magic is to select the USB host option on the SDK middleware components... ???
Now it's in the SDK build.
Oh, but it doesn't include CAN. That's only available in the binary?
Ah, so the magic is to select the USB host option on the SDK middleware components... ???
Now it's in the SDK build.