RT1064可以使用dma把GPIO数据寄存器的内容转移到内存里吗?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064可以使用dma把GPIO数据寄存器的内容转移到内存里吗?

1,432 Views
15219661324
Contributor III

RT1064如何使用使用dma把GPIO数据寄存器的内容转移到内存里?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,345 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I recommend to check section 5.4.2 for details on DMA sources. 

Performing DMA transfers to/from GPIO—Moving data from/to one or more GPIO pins, either unthrottled (that is, as fast as possible), or periodically (using the DMA triggering capability).

Performing DMA transfers from memory to the external bus, or vice-versa—Similar to memory to memory transfers, this is typically done as quickly as possible.

Please let me know if you have further questions.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply