RT1064可以使用dma把GPIO数据寄存器的内容转移到内存里吗?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064可以使用dma把GPIO数据寄存器的内容转移到内存里吗?

1,431件の閲覧回数
15219661324
Contributor III

RT1064如何使用使用dma把GPIO数据寄存器的内容转移到内存里?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,344件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I recommend to check section 5.4.2 for details on DMA sources. 

Performing DMA transfers to/from GPIO—Moving data from/to one or more GPIO pins, either unthrottled (that is, as fast as possible), or periodically (using the DMA triggering capability).

Performing DMA transfers from memory to the external bus, or vice-versa—Similar to memory to memory transfers, this is typically done as quickly as possible.

Please let me know if you have further questions.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信