RT1060 DMA request signals MUX source do not contain FlexIO3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1060 DMA request signals MUX source do not contain FlexIO3

Jump to solution
914 Views
Daniel14
Contributor III

Hi, 

Compared with RT1050, RT1060 has one more FlexIO peripherals. but I checked with IMXRT1060RM. 

RT1060 DMA request signals MUX source do not contain FlexIO3. 

So FlexIO3 can't use with DMA in RT1060? or IMXRT1060RM DMA Mux source miss FlexIO3?

Thanks for support.  

Labels (1)
0 Kudos
Reply
1 Solution
896 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Daniel14 ,

Yes, unfortunately, the FlexIO3 module is not accessible by the DMA peripheral, so you can only use the FlexIO1 and FlexIO2.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
897 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Daniel14 ,

Yes, unfortunately, the FlexIO3 module is not accessible by the DMA peripheral, so you can only use the FlexIO1 and FlexIO2.

 

Regards,

Jing

0 Kudos
Reply