RT1052CVL5B uses FLEXPWM and eDMA output and capture PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052CVL5B uses FLEXPWM and eDMA output and capture PWM

3,464 Views
purongyu
Contributor I

Hello

 

我使用 PWM1模块3的PwmA通道 在 STS[RF](Reload Flag) 置位时  触发 eDMA0通道8 写 VALX寄存器。 通过DMA0传输,使PWM1模块3的PwmA通道输出8个占空比不同、周期相同的波形,用来表示一个字节的数据,如下图表示0x04,发送的8个周期分别代表位 0000 0100。


pastedImage_3.png

随后使用 PWM2模块3的PwmA通道 捕获  上面输出的波形  来触发 DMA0通道4 读捕获寄存器。DMA0通道4 用来传输 CVAL2寄存器 的值到定义的数组; DMA0通道4 链接 通道5 来传输CVAL2CYC的值; 通道5 链接 通道6 来传输CVAL3的值;通道6 链接 通道7 来传输CVAL3CYC的值。PWM2模块3的PwmA通道 设置为 A0 下降沿捕获, A1 上升沿捕获, A0捕获 && A1捕获 触发DMA传输。

调试时,发现了几个问题:

1.   PWM1 产生波形时,有可能会丢掉第一个周期,如图:这理论上是发送 0x02(0000 0010),实际发送的却少了一个周期(000 0010)

pastedImage_4.png

2. 在PWM1发送的波形无误的情况下,PWM2捕获波形后通过DMA传输到内存的数据可能会漏掉第一个周期。如下: 图是PWM1发送的波形0x0a(00001010),是正确的;g_CVALx和g_CVALxCYC是PWM2捕获下图中波形,通过DMA传输到内存的捕获寄存器数据。出错的寄存机值见 g_CVAL2[7];g_CVAL2[7] 理论值是要比g_CVAL2[6] (26288)大,实际g_CVAL2[7]的值是初始化值7(数组初始化时赋的初始值)

pastedImage_5.png

g_CVAL2[0] = 24181 
g_CVAL2CYC[0] = 4 
g_CVAL3[0] = 24392
g_CVAL3CYC[0] = 4 


g_CVAL2[1] = 24482 
g_CVAL2CYC[1] = 4 
g_CVAL3[1] = 24692
g_CVAL3CYC[1] = 4 

g_CVAL2[2] = 24783 
g_CVAL2CYC[2] = 4 
g_CVAL3[2] = 24994 
g_CVAL3CYC[2] = 4 

g_CVAL2[3] = 25084
g_CVAL2CYC[3] = 4
g_CVAL3[3] = 25294
g_CVAL3CYC[3] = 4

g_CVAL2[4] = 25385 
g_CVAL2CYC[4] = 4 
g_CVAL3[4] = 25294     //在这里,本来DMA传输过来的应该是比 g_CVAL2[4] 大的值,结果传输的是  上一次捕获的

g_CVAL3CYC[4] = 4     //g_CVAL3[3] 的值

g_CVAL2[5] = 25987 
g_CVAL2CYC[5] = 4 
g_CVAL3[5] = 25896 
g_CVAL3CYC[5] = 4 

g_CVAL2[6] = 26288
g_CVAL2CYC[6] = 4 
g_CVAL3[6] = 26499
g_CVAL3CYC[6] = 4 

g_CVAL2[7] = 7      
g_CVAL2CYC[7] = 70      //7 和 70 是初始值,本来应该是和前面一样有正确数据的,
g_CVAL3[7] = 7                //这部分,DMA没传输数据过来
g_CVAL3CYC[7] = 70

3.  在PWM1发送的波形无误的情况下,DMA传输到内存的数据可能是上次捕获的捕获寄存器值。如上: 见 g_CVAL3[4] 和 g_CVAL3[3];g_CVAL3[4] 理论值是要比 g_CVAL3[3] (25294)大,实际g_CVAL3[4]的值等于g_CVAL3[3] 的值。

4.  在计数器从65535->0时,如果在等于0时捕获成功,则可能出现这种情况,CVAL2 捕获值为0,但CVAL2CYC捕获的值没加1.如下:g_CVAL2CYC[3] = 1,理论上应该 g_CVAL2CYC[3] = 2

g_CVAL2[1] = 64934
g_CVAL2CYC[1] = 1
g_CVAL3[1] = 65144
g_CVAL3CYC[1] = 1

g_CVAL2[2] = 65235
g_CVAL2CYC[2] = 1
g_CVAL3[2] = 65446 
g_CVAL3CYC[2] = 1

g_CVAL2[3] = 0
g_CVAL2CYC[3] = 1    //这里理论值应该是2,实际捕获到的是1
g_CVAL3[3] = 210
g_CVAL3CYC[3] = 2

g_CVAL2[4] = 300
g_CVAL2CYC[4] = 2 
g_CVAL3[4] = 391 
g_CVAL3CYC[4] = 2

5.  以上第1、2、3、点,在输出波形的频率越低时出现的概率越小,在10K时,基本上不会出现这些错误,在500k时,这些错误出现的概率就比较多了。

我估计应该是PWM的配置问题,是我哪里没有配置好吗?需要注意哪些方面?

我将我测试的代码放进附录。

Best regards,

Torstei

Labels (1)
Tags (3)
0 Kudos
Reply
7 Replies

2,945 Views
shunanli-b46639
NXP Employee
NXP Employee

purongyu‌,could you provide the "bsp_bdm.h" file? I cannot find it in your attachment.

0 Kudos
Reply

2,945 Views
purongyu
Contributor I

Hello 

My phone number:  +86 13058085495

Background of the project: This is a programmer project, this is a chip programming protocol.
The only statement in the file "bsp_bdm.h" is the test function (void BDM( void );).
Thank you for your help!

Best regards,

Aldo.

0 Kudos
Reply

2,945 Views
shunanli-b46639
NXP Employee
NXP Employee

Hi Purong,

Per our talk, you had implemented the your target fucntion by Qtimer and eDMA. Could you provide the codes of Qtimer and eDMA? Then I can compare them with that of FLEXPWM and eDMA to try to figure out the problem. Thanks!

0 Kudos
Reply

2,945 Views
purongyu
Contributor I

Hello 

抱歉,最近实在有点忙,刚刚整理了tmr实现的代码,把测试代码发上来。

有以下3个文件:

pastedImage_1.png

Best regards,

Aldo.

0 Kudos
Reply

2,945 Views
jimmychan
NXP TechSupport
NXP TechSupport

which SDK are you using?

0 Kudos
Reply

2,945 Views
purongyu
Contributor I

Hello 

The version in "fsl_edma.h" is "Version 2.1.2", as shown below:

pastedImage_4.png
The version in "fsl_pwm.h" is "Version 2.0.0", as shown below:

pastedImage_3.png
After verification, the library versions of these two modules are up to date.

Best regards,

Aldo.

0 Kudos
Reply

2,945 Views
shunanli-b46639
NXP Employee
NXP Employee

Hello purongyu

could you please provide your contact information? I want to know some background about this project. Thanks!

0 Kudos
Reply