RT1052 bypass dcdc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 bypass dcdc

879 Views
Paul8
Contributor I

大家好,近期在测试使用RT1052 MCU过程中发现,芯片的温升较高,由于结壳热阻较大,无法有效散热。尝试过降低主频,效果不明显。所以有两个问题需要咨询一下:

1、有没有有效的软件、硬件优化方法,可以降低芯片的发热

2、有没有官方的关于外挂核心供电电源的demo原理图可以提供参考。依照手册尝试了各种bypass dcdc的方案,没有成功。

谢谢,希望可以尽快得到回复

0 Kudos
Reply
1 Reply

867 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
1) 有没有有效的软件、硬件优化方法,可以降低芯片的发热
-- 针对你说的,芯片在工作时,温度过高,应该跟你板子的设计和焊接有关,我觉得你最好从这两面入手检查硬件,才能最终解决问题。
临时的方法,我建议你可以安装散热片。
2) 有没有官方的关于外挂核心供电电源的demo原理图可以提供参考。依照手册尝试了各种bypass dcdc的方案,没有成功。
-- 如果要Bypass DCDC, 仍然需要给DCDC_IN供电并将DCDC_PSWITCH接地,同时空置DCDC_LP脚。
然后选用合适的外置DCDC给VDD_SOC_IN供电,这种方案我们是很不推荐的,而且我也不认为可以解决你的问题。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply