RT1052: Can CSI VSYNC be set to falling-edge triggered?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1052: Can CSI VSYNC be set to falling-edge triggered?

1,437 次查看
udoeb
Contributor II

Hello,

The manual states in section 34.3.1.2 Gated Clock Mode:

The CSI can be programmed to support rising/falling-edge
triggered VSYNC through CSI_CR1[SOF_POL]

However, when I set SOF_POL=1 this has no effect. CSI still triggers on rising edge.

I'm using traditional interface, CCIR_EN=0, CCIR_MODE=0, EXT_VSYNC=0.

Question: How can VSYNC be configured for falling edge?

Thanks
Udo

0 项奖励
回复
3 回复数

1,414 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @udoeb ,

This is a interrupt control bit. Can you share how to test this condition?

 

Regards,

Jing

0 项奖励
回复

1,398 次查看
udoeb
Contributor II

Hi,

Thanks for your reply.

Let me rephrase the question: I do apply an external signal to VSYNC and notice that the DMA starts on the rising edge. My external circuitry requires that DMA starts on the falling edge. How can I achieve that?

Regards,
Udo

0 项奖励
回复

1,393 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

But SOF_POL default is 0, it is falling edge. SOF_POL=1 means rising edge. Opposite to your setting. So...

 

Regards,

Jing

0 项奖励
回复