RT1050 with external 16-bit low power SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 with external 16-bit low power SDRAM

1,326件の閲覧回数
matthiaspimming
Contributor I

I have configured the RT1050 to use the SEMC to interface to a external 16-bit SDRAM. The SDRAM is a Winbond 512Mb Low Power SDRAM (W989D6DB) operating at 1.8V power supply.

The SDRAM works fine most at the time, but some times it happens that the memory access fails after power up sequence. Does any one have a idea what can cause this problem?

ラベル(1)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I think, it makes sense to discuss memory (power up) initialization sequence

with memory manufacturer directly. I do not see such specs in their Datasheet.

https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信